The difference between the readback accuracy and the meter accuracy is that the readback is accurate up to the resolution of the analog-to-digital converter (ADC), but the display can only show a certain amount of digits. So, in rounding the readback value to a value that can fit in the display, there is a certain rounding error – and that error defines the meter accuracy.
When returning the readback value over the remote interface, the actual value of the ADC is returned without any rounding applied.
Applies to: All models
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |
6030A, 6031A, 6032A, 6033A, 6035A, 6038A, 6060B, 6063B, 6621A, 6622A, 6623A, 6624A, 6625A, 6626A, 6627A, 6628A, 6629A, 6641A, 6642A, 6643A, 6644A, 6645A, 6651A, 6652A, 6653A, 6654A, 6655A, 6671A, 6672A, 6673A, 6674A, 6675A, 6680A, 6681A, 6682A, 6683A, 6684A, 6690A, 6691A, 6692A, E4356A, 6611C, 6612C, 6613C, 6614C, 6631B, 6632B, 6633B, 6634B, 66309B, 66311B, 66312A, 66319B, 66319D, 66321B, 66321D, 66332A, 66000A, 66001A, 66002A, 66101A, 66102A, 66103A, 66104A, 66105A, 66106A, 6811B, 6812B, 6813B, AC6801A, AC6802A, AC6803A, AC6804A, E4360A, E4361A, E4362A, E4366A, E4367A, E4368A, E3620A, E3630A, E3631A, E3632A, E3633A, E3634A, E3640A, E3641A, E3642A, E3643A, E3644A, E3645A, E3646A, E3647A, E3648A, E3649A, E36102A, E36103A, E36104A, E36105A, E36106A, N3300A, N3301A, N3302A, N3303A, N3304A, N3305A, N3306A, N3307A, N5740A, N5741A, N5742A, N5743A, N5744A, N5745A, N5746A, N5747A, N5748A, N5749A, N5750A, N5751A, N5752A, N5761A, N5762A, N5763A, N5764A, N5765A, N5766A, N5767A, N5768A, N5769A, N5770A, N5771A, N5772A, N6700B, N6701A, N6702A, N6705A, N6705B, N6710B, N6711A, N6712A, N6715A, N6715B, N6731B, N6732B, N6733B, N6734B, N6735B, N6736B, N6741B, N6742B, N6743B, N6744B, N6745B, N6746B, N6773A, N6774A, N6775A, N6776A, N6777A, N6751A, N6752A, N6753A, N6754A, N6755A, N6756A, N6761A, N6762A, N6763A, N6764A, N6765A, N6766A, N6781A, N6782A, N6785A, N6786A, N6783A-MFG, N6783A-BDA, N6784A, N6950A, N6951A, N6952A, N6953A, N6954A, N6970A, N6971A, N6972A, N6973A, N6974A,N6976A, N6977A, N7950A, N7951A, N7952A, N7953A, N7954A, N7970A, N7971A, N7972A, N7973A, N7974A, N7976A, N7977A, N8731A, N8732A, N8733A, N8734A, N8735A, N8736A, N8737A, N8738A, N8739A, N8740A, N8741A, N8742A, N8754A, N8755A, N8756A, N8757A, N8758A, N8759A, N8760A, N8761A, N8762A, N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8937APV, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A, N8957APV, PA2201A, U8001A, U8002A, U8031A, U8032A